Network view (non-supervisor devices)

Use the
Network
settings to view network information for the port.
  • View whether the device is operating in a Linear/Star or Device-Level Ring (DLR) network.
  • View the current status of the network.
This information is only available when online, and there is no communication error in the device profile.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal