Configure limit properties
    Configure limit properties to manage the amount of data coming from an output.
To configure limit properties
- On the tab for the device, expandChannels, and then expand an individual channel.
 - In theLimitsview, fill in the parameters and selectOK.
 
Provide Feedback