View individual event properties
    Use the 
Events 
view to view event properties for the devices.To view individual event properties
- On the tab for the device, expandEvents, and then select the extended event.
 - In theEvent0xview, view the parameters for the events.TIP:To configure event properties, navigate to theTageditor.
 
Provide Feedback