Configure individual output channel properties
    Configure the individual output channel so that it can properly connect to Current or Voltage output types and to multiple output signal ranges.
To configure individual output channel properties
- On the tab for the device, expandChannels, and then select an individual channel.
 - In theCh0xview, fill in the parameters and selectOK.
 
Provide Feedback