View current channel calibration
    Use the 
Calibration 
view to view current channel calibration, including:- Channel number of the devices.
 - Calibration range value that is currently configured for the channel.
 - Calibration gain values as reported by the device.
 - Calibration offset signed values as reported by the device.
 - Last successful calibration date.
 - Calibration status per channel.
 
To view current channel calibration
- On the tab for the device, selectCalibration.
 - In theCalibrationview, view the current channel calibration.
 
Provide Feedback