Calibration Wizard parameters
    Calibration Wizard
 includes these parameters:Parameter  | Description  | 
|---|---|
Channel  | Shows the channel number to which this configuration applies.  | 
Calibrate  | Identifies the channels for calibration. Select the checkbox for the channel that you want to calibrate.  | 
Calibration Range  | Shows the value currently configured for the channel. 
  | 
Calibration Gain  | Shows the calibration gain values as reported by the device.  | 
Calibration Offset  | Shows the signed values as reported by the device.  | 
Calibration Status  | Shows the status of the calibration per channel as the calibration occurs.  | 
Low Reference  | Shows the value of the low reference signal for the channel.  | 
High Reference  | Shows the value of the high reference source based on the channel configuration.  | 
Recorded Reference  | Indicates the measured output values. For the multimeter accuracy, see the User Manual.  | 
Status  | Shows the value read during calibration for the enabled channels. 
 If  Status  shows Error , perform the corresponding actions as needed:
  | 
Provide Feedback