Calibration mismatch
    Performing calibration can cause unexpected results if:
- At least one channel is selected, and
 - There is a mismatch between the device listed in the application and the actual physical device, and
 - The system is active.
 
It is strongly recommended that you select 
No
, check the configuration, and shut down the system before performing calibration.Provide Feedback