Configure alarm properties
    Configure alarm properties to alert you when the device exceeds configured high or low limits.
To configure alarm properties
- On the tab for the device, expandChannels, and then expand an individual channel.
 - SelectAlarms.
 - In theAlarmsview, fill in the parameters and selectOK.
 
Provide Feedback