Loading

Magazine

The Journal’s August 2020 Full Issue

View and download the PDF of The Journal From Rockwell Automation and Our PartnerNetwork magazine’s print issue.

Main Image

Download the full PDF of the August 2020 print issue of The Journal From Rockwell Automation and Our PartnerNetworkTM that covers power & motor control as well as the automotive industry. Also get a preview of the 2020 Automation Fair At Home.

Editor’s Viewpoint: Virtually Everything is Going… Virtual: Executive Editor Theresa Houck describes the 2020 Automation Fair At Home event, an online experience that includes technical training, product showcases, industry forums and trade show experiences.

Cover Story: Hand Over Control: Smart drives with built-in predictive-maintenance functions do a lot of the hard work for you, making maintenance strategy easier to implement.

Ribbon Maker Cuts Manual Machine Monitoring by 30%: Automating part of its process helped this family business boost efficiency and begin producing types of ribbon that were previously not possible.

How a Toyota Engine Plant Slashed Energy Costs: New air compressor controls are saving 1 million KWh annually and support Toyota’s zero-emissions goals.

3 Keys to Future-Proofing Automotive Production: New air compressor controls are saving 1 million KWh annually and support Toyota’s zero-emissions goals.

Get Ready to Attend Automation Fair… At Home! This year’s event is online and offers a unique experience while still sharing the latest IT/OT and control technology and best practices.

How Do You Know Which Electric Linear Actuator to Use? Learn what to look for designing an electro-mechanical system to optimize food and beverage processes, including the basics of hygienic requirements.

What is an IP67-Rated Machine Vision Camera? Here’s what IP67 means, and how the IP67 rating protects a camera from dust and water ingress, temperature extremes or high shock or vibration.

 





The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Putman Media, Inc.

Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Recommended For You