Vaagen Brothers Lumber, Inc., in Colville, Washington, has a history stretching back more than 70 years. Their motto, “Small Logs. Better Lumber,” hearkens to their core principles of value and sustainability. Their facilities in Coleville and Usk, Washington, make extensive use of industrial hydraulic motion control to position saws, logs and lumber.
The company built its control systems around the Rockwell Automation Allen-Bradley® ControlLogix® programmable logic controller (PLC). For motion control of hydraulic axes, they used the 1756-M02AS and 1756-HYD02 plug-in motion modules, which served them reliably for more than 20 years.
Ryan Tietsort, an electrician at Vaagen Brothers, researched options when Rockwell Automation announced the discontinuation of the 1756-M02AE, 1756-M02AS and 1756-HYD02 analog motion modules. Among other applications, these modules had been integral to the mill’s lumber stacker system, controlling servo-hydraulic motion via the ControlLogix PLC.
With no direct replacement available from Rockwell Automation, Tietsort’s team needed an alternative that would integrate seamlessly with their existing PLC while minimizing downtime.
In addition to replacing the obsolete modules, Tietsort saw an opportunity to address a recurring issue: unstable lumber stacks. Operators frequently had to intervene manually due to inconsistencies in hydraulic motion tuning, slowing production and increasing labor costs.
The culprit wasn't mechanical failure or operator error. Rather, the issue involved less-than-ideal motion tuning with the existing system.
The Solution: Transitioning to Delta RMC Motion Controllers
After evaluating available options, the team chose Delta Motion’s RMC motion controllers as a replacement. Rockwell Automation recommends these as a replacement option because they’re compatible with Allen-Bradley PLCs and interface with the same I/O devices as the discontinued modules.