By Mike Bacidore, Contributing Editor
I recently interviewed Andrew Jaap, business manager — motion with Rockwell Automation to learn about recent developments in motors and drives and how they can help equipment builders and manufacturers. His insights are promising for industrial firms.
Bacidore: What have been the biggest improvements to motor and drives in the past five years?
Jaap: There’s a growing demand for access to machine data to better understand and improve operations, and drives are helping meet this need. The control loops in drives are faster than ever, and that gives you more access to actionable data.
Drives also have new smart capabilities like a virtual torque sensor, which uses the motor as a torque sensor to get data on what’s happening in the driven load. When this data is contextualized, it can give you insights into how your application is running.
For example, it could tell operators that a web of material might be breaking because it’s starting to thin out. The data also can give you maintenance insights, like if a mechanical drivetrain is out of adjustment, which in the past would have required external sensors and people to do data analysis.
Drives also are advancing to meet growing functional safety demands. Increasingly, a safe-torque-off safety function alone isn’t enough on a drive. It also needs functions such as safe limited torque and safe limited acceleration.
Users are increasingly looking at their applications from a system perspective, where production technologies such as robotics can move and interact more closely. Drives with safety functions support this by helping the technologies move and interact in a safe and predictable manner.
Bacidore: What’s the most innovative or efficient motor/drive application you’ve ever seen or been involved with?
Jaap: Servo drives and motors are playing a central role in helping transform operations to address challenges such as the skills gap.