3. Mistake: You use an analog signal to transport your measurement to the control system.
Strain gauge scales deliver resolution up to 100,000 increments, and Electromagnetic Force Restoration sensors deliver resolution up to 210 million increments. A 16-bit 4-20ma signal is good for a maximum of 32,000 increments. When you factor out noise and uncertainty, you might only achieve 4,000 increments of readability. This means that the analog signal reduces your readability by at least 25 times and as much as 52,000 times.
Tip: Use an automation network to transport important weight data to achieve the highest accuracy.
4. Mistake: You trust the automatic calibration feature, but don’t confirm results with weights.
Many people are tricked by the idea of not using test weights. Automatic calibration features do not actually “test” the scale to confirm operation; they only adjust the scale to known default values for easy setup. Only test weights, or hydraulic calibration, prove that shipping hardware has been removed, that there is nothing blocking the scale, and that all sensors are transmitting accurate measurements.
Automatic calibration is a useful tool for quickly configuring your system, but when you really want to prove fit for purpose, it’s necessary to confirm your scale is accurate (true and repeatable). Routine calibration after initial calibration confirms that your scale continues to provide accurate measurements.
Tip: Physical calibration identifies broken components, cables or load cells.
5. Mistake: You use a noncompliant automation interface.
The Open Device Vendors Association (ODVA), for example, specifies and tests products to verify they’ll function well on EtherNet/IP™ networks. Compliance sets the basis for easy installation and consistent, trouble-free operation; not all manufacturers and equipment are compliant.
When you select a weighing device or use a gateway, make sure 1) it has a specific (not generic) conformance certificate, and 2) it meets your data throughput requirements.
Tip: Go to www.odva.org and confirm that a product conformance certificate is available. Make sure you have the EDS, AOP or other important drivers.
Scale and Network Components
These tips can help you avoid some of the most common mistakes we’ve seen across several weighing applications, and help make your project run a lot more smoothly. Remember to select the right scale and network components based on your production and automation requirements, calibrate by physical methods, review your control philosophy with an expert, and select modern products with condition monitoring and advanced filtering.
Based in Switzerland with North American headquarters in Columbus, Ohio, METTLER TOLEDO is a Technology Partner in the Rockwell Automation PartnerNetwork™ ecosystem. The company provides weighing solutions that include industrial weigh modules, load cells and PLC connectivity devices that easily integrate weight into automated applications.
Like this article? Sign up for the digital magazine from The Journal From Rockwell Automation and Our PartnerNetwork and get articles like this delivered right to your inbox.
The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Endeavor Business Media.