By Dennis Nash, President & CEO, Control Station, Inc.
Editor’s Note: This article is adapted from the white paper, “Successfully Optimizing Regulatory Controllers Without Risking Data Security.” Download the full paper at https://bit.ly/tj0123cswp to get information about the pitfalls of historical data and some challenges of using live data. Learn how to use “live-historical” data captured via FactoryTalk® Linx and delivered via the FactoryTalk Live Data interface, and get step-by-step instructions on how to tune PIDs using live-historical data.
The PID controller has been a fixture in manufacturing for decades. From the simple to the complex, the PID remains the primary resource used to regulate industrial production processes. Just as the methods and the tools used to automate production have evolved over the years, so too has the data used in loop tuning and process optimization.
In the past, production and engineering staff performed manual tuning, using analog data to visually estimate the values that would provide the basis for calculations of Gain, Dead-Time, and Time Constant. Manual tuning is still performed today, and although the available data is better, most outcomes are only marginally improved.
Then PID tuning software facilitated a more methodical approach for assessing process data, generating models and calculating parameters. While these early tuning products were limited to uploading and analyzing files, they eventually gained the ability to communicate directly with controllers and access live data.