Expanded high-performance portfolio helps reduce system complexity, enhance operational productivity and shorten development time for smart machines
CHICAGO, Nov. 18, 2015 — Smart manufacturing is driving a demand for connected machines and equipment. Adding more devices and connections, however, can make machines and systems more complex. The expanded next-generation Integrated Architecture portfolio from Rockwell Automation reduces complexity while helping users meet future capacity and throughput needs as they design systems for a Connected Enterprise.
The portfolio includes a newly released next-generation Allen-Bradley controller, graphic terminal, servo drive and distributed I/O system, as well as the latest release of the Rockwell Software Studio 5000 and FactoryTalk software offerings.
“We’ve invested significantly in the Integrated Architecture portfolio to help our customers prepare their production environments for future growth, and help machine builders simplify machines and get them to market faster,” said Dan DeYoung, market development director, Integrated Architecture, Rockwell Automation. “With this new portfolio and our ongoing collaboration with our PartnerNetwork members, customers have the tools to more easily design, operate and maintain smart, high-performing systems.”
The new additions to the portfolio include:
- The latest release of the Studio 5000 software includes three new applications: Studio 5000 Architect, Studio 5000 View Designer and Application Code Manager. These applications, along with the Studio 5000 Logix Designer application released in 2012, bring more functionality together into one environment to simplify and speed system development. In addition, the latest releases of FactoryTalk ViewPoint Mobile software and FactoryTalk VantagePoint Mobile software allow users to more easily engage with their production information on mobile devices.
- The Allen-Bradley ControlLogix 5580 controller provides up to 45 percent more application capacity and includes an embedded 1-gigabit Ethernet port to support high-performance communications, I/O and applications with up to 256 axes of motion. The new port and additional capacity cuts the amount of control and communications hardware required, reducing system complexity, costs and required panel space.
- The Allen-Bradley Kinetix 5700 servo drive is a single-platform alternative to using multiple servo drives for large custom machines with high axis-count and power requirements. This can reduce cabinet-space requirements by up to 70 percent and wiring requirements by as much as 60 percent.
- The Allen-Bradley Bulletin 5069 Distributed Compact I/O system with two 1-gigabit Ethernet ports scans 10 times faster than previous versions for greater productivity. The system can connect to as many as 31 modules without the need to expand.
- The Allen-Bradley PanelView 5500 graphic terminal provides a modern design and enhanced integration with Logix controllers using the Studio 5000 View Designer application. This integration improves programming efficiency because engineers can enter configuration information once and use it for the entire automation design.
The expanded portfolio also incorporates a number of security features to help manufacturers and industrial operators protect their facilities, assets and intellectual property.
News Release Assets
Images available upon request or here at box.com.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs about 22,500 people serving customers in more than 80 countries.
Media Contacts
Paul Whitney
Rockwell Automation
414.382.3696
pwwhitney@ra.rockwell.com
Leanne Hanson
PadillaCRT
612.455.1776
leanne.hanson@padillacrt.com
Allen-Bradley, Bulletin 5069, Compact I/O, ControlLogix, FactoryTalk, Integrated Architecture, Kinetix, LISTEN. THINK. SOLVE., PanelView, PartnerNetwork, Rockwell Software, Studio 5000, Studio 5000 Architect, Studio 5000 Logix Designer,Studio 5000 View Designer and VantagePoint are trademarks of Rockwell Automation Inc.
Published November 17, 2015