Loading
Press Release | July 23, 2018
Recent ActivityRecent Activity

Brighter, More Flexible Tower Light Now Available from Rockwell Automation

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail

Tower light accommodates seven modules in same stack for ease of use and selection

MILWAUKEE — Rockwell Automation introduces the Allen-Bradley ControlTower 856T 70 mm Tower Light system. This new system incorporates brighter LED illumination and a broad offering of visual and sound technologies all in a 70 mm diameter housing. The ControlTower 856T is capable of accommodating up to seven modules in the same stack, offering users the ability to monitor more machine and process conditions in a single device.

This new modular design allows the ControlTower 856T system to meet the widest range of signaling applications with a reduced number of components.

project scio



Click to download image.

“Our new tower light helps engineers achieve faster time to market due to the reduced number of components they need to select,” said Alvaro Sanchez, product manager, Rockwell Automation. “Users may also see a lower total cost of ownership due to the scalable visual and audible options and the ability to monitor more machine conditions with a single tower light.”

The tower light features push-in terminal blocks in the base and internal DIP switches inside the light and sound modules that enable engineers to easily configure operation modes. Engineers can choose from a range of sounds that help alert operators on a machine’s status or condition. These sound options include multi-tone piezoelectric, multi-tone transducer technologies.

The ControlTower 856T system also includes non-stackable, beacon-shaped light modules for those applications that require a low profile signaling device but want to use the same mounting infrastructure of the tower light.

The IP66/67-rated system can be used in tough environmental conditions and in an extended operating temperature (up to 70 degrees Celsius). To meet global requirements, the system is available in 24V AC/DC and 120/240V AC. The product line is available as separate components or as a pre-configured, factory-assembled stack light for optimal flexibility.

About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries.

Media Contacts
Todd Bissell
Rockwell Automation
978.446.3284
tmbissel@ra.rockwell.com

Heidi Wight
Padilla
612.455.1795
Heidi.Wight@padillaco.com

Allen-Bradley and ControlTower are trademarks of Rockwell Automation Inc.

Published July 23, 2018


  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Press Releases
  5. Chevron LeftChevron Left Brighter, More Flexible Tower Light Now Available from Rockwell Automation