What is Allowlisting
Allowlisting is a proactive cybersecurity strategy that blocks unauthorized programs from running by allowing only pre-approved applications to execute. It operates on a “default deny” principle, meaning anything not explicitly permitted is automatically restricted. This approach aligns perfectly with the predictable and static nature of OT environments and offers a tailored solution for securing industrial systems.
The Benefits of Allowlisting in OT
- Stronger Threat Prevention: Block unauthorized applications, allowlisting neutralizes zero-day exploits and APTs before they can take hold.
- Reduced Attack Surface: Limit the software that can run minimizes potential entry points for attackers.
- Operational Stability: Prevent unapproved changes or software installation protects system integrity and reduces the risk of downtime.
- Simplified Compliance: Streamline adherence to industry standards and frameworks like NIST, IEC 62443, and NERC CIP.
Increased Security Efficiency: By allowing only approved applications, you cut down the effort spent chasing countless alerts and monitoring every possible threat—freeing resources for higher-value security initiatives.
Alignment with Zero Trust Principles: It enforces a “never trust, always verify” approach, ensuring every application is vetted before execution.
For organizations operating in the OT space, allowlisting represents not just an alternative to antivirus, but a paradigm shift in how security is approached—proactively and with the unique needs of industrial environments in mind.
How to Secure Your OT Environment with Application Allowlisting
Implementing application allowlisting requires careful planning and execution. This five-step process provides a proven approach for successful deployment:
Step 1: Lay the Foundation for Success
Creating a comprehensive deployment plan is essential. This involves:
Asset Inventory
Conduct a thorough inventory of all hardware and software in your OT environment. This includes operating systems, applications, firmware versions, and network connections. A detailed asset inventory checklist should include: device name, IP address, OS, installed software, function, criticality.
Tool Selection
Evaluate different application allowlisting tools based on features, compatibility with your OT systems (including legacy systems), management capabilities, and integration with existing security infrastructure.
Compatibility Assessment
Determine which systems can be protected. Most modern tools support Windows XP SP3 and later. For older systems (Windows NT, Server 2000), consider mitigation strategies like network segmentation, virtual patching, or, if possible, upgrades.
Deployment Method
Choose the appropriate deployment method:
- Remote Agent Deployment: Use existing system management tools like BigFix, SCCM, Active Directory, or specialized technology like SecureOT Platform
- Manual Installation: For systems without remote management capabilities, schedule on-site visits with operators, respecting change management procedures.
Change Management
Engage with OT operators early in the process and follow established change management procedures to minimize disruption to operations.
Performance Impact Assessment
Evaluate the potential performance impact of the allowlisting agent on HMIs and servers. Most modern solutions have minimal impact, but testing is crucial.
Soak Testing
Select representative systems for initial testing (“soak testing”). These should be non-critical systems that mirror production environments.
Step 2: Establish a Gradual and Controlled Rollout
When introducing new security measures, a careful and deliberate approach is key to success.
Phased Deployment
Begin by deploying the allowlisting agent to a small number of systems, following a “low and slow” approach to minimize network congestion and potential disruptions.
Disabled Mode Deployment
Crucially, deploy the agents in disabled (or monitoring) mode. This allows the agent to collect information about running applications without actively blocking anything. This prevents operational disruptions during initial setup. Tamper protection, while important, can cause issues if communication with the allowlisting server is interrupted.
Testing in a Non-Production Environment
If possible, replicate a section of your OT network in a test environment to thoroughly test the deployment and configuration before implementing changes in production.
Step 3: Build an Accurate Allowlist
- Simulation Mode: After deployment, transition the agents to simulation mode. This allows the agent to log all file execution attempts without blocking them, generating a comprehensive log of application usage.
- Log Analysis: Analyze the simulation logs to identify legitimate applications that need to be allowlisted and any potential false positives (legitimate applications mistakenly flagged as unauthorized).
- Collaboration with Operations: Work closely with OT operators to understand the legitimate use of applications and identify any unusual activity.
- Duration: The simulation phase should last for a sufficient period (typically a few weeks) to capture all regular system activity and ensure an accurate allowlist.
- Alert Configuration: Configure alerts to track blocked files during simulation. This helps validate the allowlist during the lockdown phase.
Step 4: Define Approved Applications
In order to create an effective allowlisting policy, it's essential to define exactly which applications are trusted.
Allowlisting Methods
For the highest level of security, you can prioritize allowlisting based on trusted software publishers. This is the safest method because it only allows digitally signed and verified software to run on your systems.
Alternatively, path-based allowlisting uses file paths to approve applications located in specific directories. This method is helpful for custom applications or software that doesn't have a digital signature.
You can also use hash-based allowlisting to identify and approve specific file versions using cryptographic hashes. This offers the most granular control, but it may require more management whenever software is updated.
Granular Rules
Create separate allowlists for different types of systems (e.g., HMIs, engineering workstations, servers) to ensure only necessary applications are allowed on each.
Handling Unsigned Applications
For unsigned or custom applications, carefully evaluate their legitimacy and consider using hash-based allowlisting or creating exceptions based on file paths.
Trusted Directories
Create “trusted directories” for software updates and patches. Installer files placed in these directories are automatically approved by the allowlisting server, simplifying the update process. This feature should be enabled only when needed and disabled after the update is complete.
Step 5: Enforce the Allowlist
- Phased Lockdown: Begin the lockdown phase by moving the previously selected “soak test” systems into lockdown mode.
- Monitoring and Alerting: Closely monitor the systems in lockdown mode and respond promptly to any alerts indicating blocked applications.
- Allowlist Adjustments: If legitimate applications are blocked, update the allowlist accordingly.
- Gradual Rollout: Once the allowlist is validated on the test systems, gradually roll out the lockdown to the remaining systems, following the “low and slow” approach.
- Ongoing Maintenance: Regularly review the allowlisting rules and logs to ensure continued effectiveness and adapt to any changes in the OT environment.
The success of this approach lies in its proactive nature. Unlike traditional reactive security methods, application allowlisting anticipates potential threats and blocks them before they can compromise critical systems. When implemented correctly, this strategy not only strengthens the overall security framework but also supports regulatory compliance and operational continuity. In a world of evolving cyber threats, allowlisting offers OT environments a dependable and future-ready defense.
Common Concerns About Application Allowlisting in OT
Rolling out new security measures often sparks questions and concerns, and application allowlisting is no exception. Organizations might worry about hurdles such as the complexity of setup, the risk of disrupting operations, potential costs, or the effort involved in managing software updates. While these are valid considerations, practical solutions exist to address each of them. Let’s break them down.
Complexity
While initial setup requires planning, modern allowlisting solutions are specifically designed to simplify deployment, streamline ongoing maintenance, and provide centralized management consoles. These features directly address the need for efficient, easy-to-manage tools. Managed security services can also provide expert support.
Operational Disruption
Proper planning, testing, and collaboration with operations teams minimize the risk of disruption. The simulation phase is crucial for identifying and addressing potential conflicts before lockdown.
Cost
While there is an initial investment, the cost of implementing application allowlisting is often significantly less than the potential cost of a security incident, including downtime, data loss, and reputational damage.
Software Updates
Trusted directories and flexible rule creation allow for seamless software updates and patching within an allowlisting framework.
Embracing Application Allowlisting for a Safer Future
Application allowlisting is more than just an alternative to antivirus tools in OT environments—it’s a significant step toward proactive and preventative security. Rather than attempting to keep up with an endless stream of new threats, allowlisting takes a different approach by permitting only verified and trusted applications to operate. This shift provides robust defense against zero-day attacks, simplifies operations, and meets the specific needs of industrial control systems.
Adopting allowlisting does come with its challenges. Concerns such as setup complexity, potential disruptions, costs, or the management of software updates are valid, but they are not insurmountable. With careful planning, gradual implementation, and the help of modern tools designed to simplify the process—like those offering trusted directory features—these obstacles can be addressed effectively. The five-step guide shared earlier offers organizations a clear path to transition smoothly to this model.
Given the evolving threat landscape, OT organizations need to move beyond reactive measures to safeguard critical systems. By adopting allowlisting, IT/OT security managers can strengthen operational continuity, reduce the cost of downtime, and build a more resilient organization. The question isn’t whether allowlisting should be implemented but how soon it can be adopted. Taking this step now can help protect vital operations and create a more resilient, secure future for your organization.