Install Redundant Chassis Components

When you install redundant chassis components, be sure to match the slot locations of partner modules in each redundant chassis.
IMPORTANT:
Do not power on either chassis until you have installed all modules in both chassis.
  1. Install the power supply or redundant power supplies for the first chassis.
  2. Install and connect the redundancy modules in both chassis.
  3. Install
    EtherNet/IP
    communication modules in the first chassis.
  4. Install one controller in the first chassis.
  5. Install the power supply or redundant power supplies in the second chassis.
  6. Install the second chassis
    EtherNet/IP
    communication modules.
  7. Install one controller in the second chassis of the redundant pair.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal