Use the Controller Status Menu to Download to the Controller

After you select a communication path in the Logix Designer application, you can use the Controller Status menu to download to the controller.
From the Controller Status menu, choose Download. After the download completes, the project name appears on the scrolling status display.
Download via the Controller Status Menu
This image shows how to download a project in Logix Designer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal