Browse Logic dialog box

Use the
Browse Logic
dialog box to browse all of the comments related to logic in the project.
TIP: To open the Browse Logic dialog, select
Search > Browse Logic
.
The following table describes the parameters in the dialog box.
Parameter
Description
Find
Used to specify the logic to search for. You can limit your search by specifying the name of a project component in the Logic list.
Logic
Lists the types of logic to browse, such as programs, routines,
Equipment Phase
s,
Equipment Sequence
s, and Add-On-Instructions. Click
+
to expand the list to show routines for the logic. To open a logic editor, double-click an element of logic such as a rung in ladder logic, a line of structured text, or a step or transition in an
Equipment Sequence
diagram.
TIP: If you change the order of sheets in the
Function Block Editor
, the sheets are renumbered and reordered in the Logic list.
Description
Displays the description of the logic.
Go To
Used to navigate to the place in the project where the logic resides.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal