No support of Ethernet port configured modules with redundancy
For the ControlLogix 5580, GuardLogix 5580, and ControlLogix 5590 controllers, redundancy
does not support modules under the controller's Ethernet front port. Select
OK
and
remove all modules under the controller's Ethernet front port in the I/O configuration. Provide Feedback