Failed to set modify trend properties - Time Period out of range

The
Time Period
is invalid. Enter a valid
Time Period
in the range from 0 to 1000 * the specified
Sample Period
.
The maximum range for
Time Period
is limited to 1000 samples worth of data. Determine
Max Time Period
by multiplying the
Sample Period
(on the
Sampling
tab) times 1000 Samples.
Example: 10ms/Sample * 1000Sample * 1Sec/1000ms = 10 Seconds
The minimum range is zero.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal