Danger: Changing <program> to a Folder will Unschedule It
You are attempting to change a program to a folder while the system is online. Changing a program that is scheduled to a folder unschedules the program and may have unintended consequences. It also removes the program from the
Controller Organizer
, because folders appear only in the Logical Organizer.
Select
OK
to change the program to a folder, or select Cancel
to leave the program unchanged.Provide Feedback