Edit SFC Element > Converge Sequences command

Choose this command to wire the selected elements together to create a branch convergence.
If you have two or more transitions selected, choosing this command creates a selection branch convergence. If you have two or more steps selected, choosing it creates a simultaneous branch convergence.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal