Error reading the list of running drivers from FactoryTalk Linx
This error occurs after shutting down
FactoryTalk Linx
while the Logix Designer
application is still running, and then selecting a
driver in the application. Shut down and restart the application.This error also occurs if
FactoryTalk Linx
is not installed, or if there is a
problem with the FactoryTalk Linx
installation on the computer.For assistance with
FactoryTalk Linx
, contact Rockwell Automation
Technical Support.Provide Feedback