Select a file name for an imported project
To select a file name for an imported file:
- In theLook Infield, enter or browse for the folder in which you wish to save the project.
- In theFile Namefield, enter the name of the project file into which you wish to import the .L5K file.
- In theFiles of Typefield, be sure to select the .ACD file type.
- If you wish to save the project as a different revision, choose the revision you wish to use from theTo:pull-down menu in the lower left portion of the dialog box.Note that this revision refers to the version of theLogix Designerapplication. TheFrom:field displays the software revision for which the project is currently configured.
- ClickImportto import into the project file you have specified.If you have changed the revision information for this project, then the version of theLogix Designerapplication that is compatible with the project’s revision is launched, the file is imported and saved, and any errors that may have occurred are displayed.
Provide Feedback