New Folder Dialog Box Overview
Use this dialog box to create a new folder within the source control database.
Parameters
Parameter | Description |
|---|---|
Name | Enter the name of the new folder. |
Comments | Enter a comment up to 255 characters in length. Comments longer than 255 characters are truncated. |
OK | Create the new folder within source control. |
Cancel | Return to the Add Project to Source Control dialog box without creating the new folder. |
Help | Help on this dialog box. |
Provide Feedback