Motion Run Hookup Diagnostics (MRHD)
This information applies to the
CompactLogix
5370, ControlLogix
5570, Compact GuardLogix
5370, GuardLogix
5570, Compact GuardLogix
5380, CompactLogix
5380, ControlLogix
5580, GuardLogix
5580, and ControlLogix 5590 controllers. Controller
differences are noted where applicable.Use the Motion Run Hookup Diagnostics (MRHD) instruction to command the motion module to run any one of three different diagnostics on the specified axis as selected by the Diagnostic Test. Currently diagnostics are available to test the motor/encoder hookup for a servo axis, the encoder hookup, and the encoder marker hookup. Commutation Test is also available but only on an AXIS_CIP_DRIVE axis. Only the motor/encoder diagnostic initiates motion on the axis. This action consists of a short move of a user Motor Encoder Test Increment. The move is initiated by roughly 1 Volt per second ramping level of the servo’s drive output. The result of executing the MRHD instruction is that the parameters, Test Status and Test Direction Forward are updated.
- This is a transitional instruction. Follow these steps when using it:
- In ladder logic, insert an instruction to toggle the rung-condition-in from false to true each time the instruction should execute.
- In a Structured Text routine, insert a condition for the instruction to cause it to execute only on a transition.
Available Languages
Ladder Diagram

Function Block
This instruction is not available in function block.
Structured Text
MRHD(Axis,MotionControl,DiagnosticTest);
Operands
There are data conversion rules for mixed data types within an instruction. See Data Conversions.
Ladder Diagram and Structured Text
Operand | Type CompactLogix 5370, Compact GuardLogix 5370, Compact GuardLogix 5380, CompactLogix 5380 | Type ControlLogix 5570, GuardLogix 5570, ControlLogix
5580, GuardLogix 5580, and ControlLogix 5590 controllers | Format | Description |
Axis | AXIS_CIP_DRIVE | AXIS_CIP_DRIVE AXIS_SERVO AXIS_SERVO_DRIVE REF_TO_AXIS_CIP_DRIVE REF_TO_AXIS_SERVO REF_TO_AXIS_SERVO_DRIVE | Tag | Name of the axis on which to perform the operation. For controllers that support
the REF_TO motion data types, the supported axis operand type can be replaced by
an equivalent REF_TO type. |
Motion Control | MOTION_INSTRUCTION | MOTION_INSTRUCTION | Tag | Structure used to access instruction status parameters. |
Diagnostic test | DINT | DINT | Immediate | Selects the specific test for the motion module to run: 0 = motor/encoder hookup test 1 = encoder hookup test 2 = encoder marker test 3=commutation test |
See Structured Text Syntax for
more information on the syntax of expressions within structured text.
For the operands that require you to select from available options, enter your selection as:
This Operand | Has These Options Which You | |
Enter as Text | Or Enter as a Number | |
DiagnosticTest | motor_encoder encoder marker commutation | 0 1 2 3 |
MOTION_INSTRUCTION Structure
Mnemonic | Description |
.EN (Enable) Bit 31 | It is set when the rung makes a false-to-true transition and remains set until the servo message transaction is completed and the rung goes false. |
.DN (Done) Bit 29 | It is set after the hookup test apply process has been successfully executed. |
.ER (Error) Bit 28 | It is set to indicate that the instruction detected an error, such as if you specified an unconfigured axis. |
.IP (In Process) Bit 26 | It is set on positive rung transition and cleared after the diagnostic test process is complete, or terminated by a stop command, shutdown, or a servo fault. |
.PC (Process Complete)Bit 27 | It is set after the diagnostic test process has been successfully completed. |
Description - AXIS_SERVO, AXIS_SERVO_DRIVE
The MRHD instruction is used to execute various test diagnostics on the specified axis to test the integrity and, in some cases, the polarity of servo field connections. There are currently test diagnostics supporting drive hookup, encoder hookup, marker hookup and motion module OK contact hookup. Test for Commutation also available when using Axis_CIP_Drive. During some of these test processes the motion module generates output to the external drive to produce a small amount of motion. Measurements made during some of these hookup diagnostic tests are saved as output configuration parameters that also serve as input data for a subsequent MAHD (Motion Apply Hookup Diagnostic) instruction. MRHD requires only one explicit input parameter, Diagnostic Test. Enter or select the Diagnostic Test to run and the axis to test.
If the targeted axis does not appear in the list of available axes, the axis has not been configured for operation. Use the Tag Editor to create and configure a new axis.
The MRHD instruction uses axis configuration parameters as input and output. The input configuration parameters that MRHD uses are shown in this table.
Axis Parameter | Data Type | Units | Meaning |
Motor Encoder Test Increment | Real | - | Distance that the Axis must travel to satisfy the Hookup Diagnostic Test. |
The axis configuration parameters that MRHD generates as output depend on the specified Hookup Diagnostic.
Motor Encoder Hookup Test
If the Motor Encoder Test is selected, the motion module enables the external drive and generates a 1 Volt per second output ramp to the drive while monitoring the encoder feedback. When the axis has moved a distance greater than or equal to the configured Motor Encoder Test Increment, the test voltage is set back to zero and the drive disabled. The motion module then reports the direction of travel which is stored as one of these output parameters:
Axis Parameter | Data Type | Units | Meaning |
Test Status | Integer | - | Status Report of the Hookup Diagnostic Test Process. |
Test Direction Forward | Boolean | - | Direction of axis travel during hookup test as seen by the motion module. |
If due to improper hookup, or some other problem with the system, the axis feedback fails to detect that axis reaching the configured Motor Encoder Test Increment within 2 seconds, the servo sets the test voltage back to zero and disables the drive. The control reflects this condition through the Test Status axis output parameter. This usually indicates that either the cabling to the drive or the cabling to the encoder is incorrect. Running MRHD with the Encoder Hookup Test selected is an effective method of isolating the problem to the encoder or drive.
Encoder Hookup Test
If the Encoder Test is selected, the motion module does not generate any axis motion, but simply monitors axis encoder feedback. The axis can then be moved by hand or by some other independent drive actuator to generate motion. When the motion module detects that the axis has moved a distance greater than or equal to the configured Motor Encoder Test Increment, the test is complete. The motion module then reports the direction of travel as one of the following MRHD output parameters.
Axis Parameter | Data Type | Units | Meaning |
Test Status | Integer | - | Status Report of the Hookup Diagnostic Test Process. |
Test Direction Forward | Boolean | - | Direction of axis travel during hookup test as seen by the motion module. |
If due to improper hookup, or some other problem with the system, the axis feedback fails to detect the axis reaching the configured Motor Encoder Test Increment after moving the axis at least that distance, then abort the test using the MAS instruction and check the encoder wiring.
Marker Hookup Test
If the Marker Test is selected, the motion module does not generate any axis motion, but simply monitors axis encoder feedback. The axis can then be moved by hand or by some other independent drive actuator to generate motion. When the motion module detects a marker (Channel Z) pulse, the test is then complete. The motion module then reports success via the Test Status.
Axis Parameter | Data Type | Units | Meaning |
Test Status | Integer | - | Status Report of the Hookup Diagnostic Test Process. |
Test Direction Forward | Boolean | - | Direction of axis travel during hookup test as seen by the motion module. |
If due to improper hookup, or some other problem with the system, the axis feedback fails to detect that axis reaching the configured Motor Encoder Test Increment after moving the axis at least that distance, then abort the test using the MAS instruction and check the encoder wiring.
Test Status
Conditions may occur that make it impossible for the control to properly perform the test operation. When this is the case, the test process is automatically aborted and a test fault is reported and stored in the Test Status output parameter. It is also possible to manually abort a test process using a MAS instruction which results in a test fault reported by the Test Status parameter. Possible values for Test Status are shown in the table below:
Error Message | Code | Definition |
Test Success | 0 | Test Process has been successful. |
Test In Process | 1 | Test is in progress. |
Test Aborted | 2 | Test Process was aborted by user. |
Test Time-out | 3 | Test Process has exceeded timed out (2 seconds). |
Test Servo Fault | 4 | Test Process Failed due to Servo Fault. |
Test Increment Fault | 5 | Test Process Failed due to insufficient test increment distance to make a reliable measure. |
To successfully execute a MRHD instruction running the Motor Encoder Test, the targeted axis must be configured as a Servo Axis Type and the axis must be in the Axis Ready state. For other tests this instruction executes properly on either a Servo or Feedback Only axis type. If any of these conditions are not met than the instruction errs.
IMPORTANT:
When the MRHD instruction is initially executed the In process (.IP)
bit is set and the Process Complete (.PC) bit is cleared. The MRHD instruction execution can
take multiple scans to execute because it requires transmission of multiple messages to the
motion module. The Done (.DN) bit, is not set immediately, but after these messages are
successfully transmitted. The In process (.IP) bit is cleared and the Process Complete (.PC)
bit is set at the same time that the Done (.DN) bit is set.
Description - AXIS_CIP_DRIVE
The MRHD instruction is used to execute various test diagnostics on the specified CIP axis to test the integrity and, in some cases, the polarity of servo field connections. There are currently test diagnostics supporting drive hookup, encoder hookup, marker hookup and motor commutation hookup. During some of these test processes, the motion module generates output to the external drive to produce a small amount of motion. Measurements made during some of these hookup diagnostic tests are saved as output configuration parameters. MRHD requires only one explicit input parameter, Diagnostic Test. Enter or select the Diagnostic Test to run and the axis to test.
If the targeted axis does not appear in the list of available axes, the axis has not been configured for operation. Use the Tag Editor to create and configure a new axis.
The MRHD instruction uses the CIP axis configuration parameters as input and output. The input configuration parameters that the MRHD uses are shown in this table.
Axis Parameter | Data Type | Units | Meaning |
Hookup Test Distance | Real | Position Units | Distance that the axis must travel to satisfy the selected hookup test process. |
Hookup Test Time | Real | Seconds | Time that the axis must continue moving to satisfy the selected hookup test |
Hookup Test Feedback Channel | USINT | - | Used by the Hookup Test service when the encoder test is selected to determine which feedback channel to test 1 = Feedback 1 2 = Feedback 2. |
The CIP axis configuration parameters that MRHD generates as output depend on the specified Hookup Diagnostic.
Motor Encoder Hookup Test
The Motor Encoder Hookup test is selected, the motion module enables the external drive and generates a 1 Volt per second output ramp to the drive while monitoring the encoder feedback. When the axis has moved a distance greater than or equal to the configured Motor Encoder Test Increment, the test voltage is set back to zero and the drive is disabled. The motion module then reports the direction of travel that is stored as one of these output parameters.
Axis Parameter | Data Type | Units | Meaning |
Hookup Test Status | USINT | - | Returns the status of the last Run Hookup Test service on the targeted drive
axis. The Hookup Test Status attribute can be used to determine when the hookup
test service has successfully completed. Conditions may occur, however, that make it impossible for the drive to properly perform the operation. When this is the case, the test process is automatically terminated and a test error is reported that is stored in the Hookup Test Status output parameter. 0 = test process successful 1 = test in progress 2 = test process aborted 3 = test process timed-out 4 = test process faulted 5 = test failed - no feedback 1 counts 6 = test failed - no feedback 2 counts 7-127 = reserved 128 = test not allowed in Axis Test Mode 129-255 = reserved 2 |
Hookup Test Feedback Direction 1 | USINT | - | Reports the direction of axis travel during the last hookup test, as detected by the drive's feedback 1 device. 0 = The drive’s feedback 1 device detected a positive direction, that is, increasing counts. 1 = The drive’s feedback 1 device detected a negative direction, that is, decreasing counts. 2-255 = reserved The value for Hookup Test Feedback 1 Direction, as determined by the hookup test, does not depend on the current feedback, motor, or motion polarity attribute configuration. This value, combined with the user’s definition of forward direction, can be used to configure the various polarity attributes for the correct directional sense. |
Hookup Test Feedback Direction 2 | USINT | - | Reports the direction of axis travel during the last hookup test, as detected by the drive's feedback 2 device. 0 = The drive’s feedback 2 device detected a positive direction, that is, increasing counts. 1 = The drive’s feedback 2 device detected a negative direction, that is, decreasing counts. 2-255 = reserved The value for Hookup Test Feedback 2 Direction, as determined by the hookup test, does not depend on the current feedback, motor, or motion polarity attribute configuration. This value, combined with the user’s definition of forward direction, can be used to configure the various polarity attributes for the correct directional sense. |
If due to improper hookup, or some other problem with the system, the axis feedback fails to detect the axis reaching the configured Motor Encoder Test Increment within 2 seconds, the servo sets the test voltage back to zero and disables the drive. The control reflects this condition through the Test Status axis output parameter. This usually indicates that either the cabling to the drive or the cabling to the encoder is incorrect. Running MRHD with the Encoder Hookup Test selected is an effective method of isolating the problem to the encoder or drive.
Encoder Hookup Test
If the Encoder Test is selected, the motion module does not generate any axis motion, but simply monitors axis encoder feedback. The axis can then be moved by hand or by some other independent drive actuator to generate motion. When the motion module detects that the axis has moved a distance greater than or equal to the configured Motor Encoder Test Increment, the test is complete. The motion module then reports the direction of travel as one of these MRHD output parameters:
Axis Parameter | Data Type | Units | Meaning |
Hookup Test Status | USINT | - | Returns the status of the last Run Hookup Test service on the targeted drive
axis. The Hookup Test Status attribute can be used to determine when the hookup
test service has successfully completed. Conditions may occur, however, that make it impossible for the drive to properly perform the operation. When this is the case, the test process is automatically terminated and a test error is reported that is stored in the Hookup Test Status output parameter. 0 = test process successful 1 = test in progress 2 = test process aborted 3 = test process timed-out 4 = test process faulted 5 = test failed - no feedback 1 counts 6 = test failed - no feedback 2 counts 7-127 = reserved 128 = test not allowed in Axis Test Mode 129-255 = reserved 2 |
Hookup Test Feedback Direction 1 | USINT | - | Reports the direction of axis travel during the last hookup test, as detected by the drive's feedback 1 device. 0 = The drive’s feedback 1 device detected a positive direction, that is, increasing counts. 1 = The drive’s feedback 1 device detected a negative direction, that is, decreasing counts. 2-255 = reserved The value for Hookup Test Feedback 1 Direction, as determined by the hookup test, does not depend on the current feedback, motor, or motion polarity attribute configuration. This value, combined with the user’s definition of forward direction, can be used to configure the various polarity attributes for the correct directional sense. |
Hookup Test Feedback Direction 2 | USINT | - | Reports the direction of axis travel during the last hookup test, as detected by the drive's feedback 2 device. 0 = The drive’s feedback 2 device detected a positive direction, that is, increasing counts. 1 = The drive’s feedback 2 device detected a negative direction, that is, decreasing counts. 2-255 = reserved The value for Hookup Test Feedback 2 Direction, as determined by the hookup test, does not depend on the current feedback, motor, or motion polarity attribute configuration. This value, combined with the user’s definition of forward direction, can be used to configure the various polarity attributes for the correct directional sense. |
If due to improper hookup, or some other problem with the system, the axis feedback fails to detect the axis reaching the configured Motor Encoder Test Increment after moving the axis at least that distance, then abort the test using the MAS instruction and check the encoder wiring.
Marker Hookup Test
If the Marker Test is selected, the motion module does not generate any axis motion, but simply monitors axis encoder feedback. The axis can then be moved by hand or by some other independent drive actuator to generate motion. When the motion module detects a marker (Channel Z) pulse, the test is then complete. The motion module then reports success via the Test Status.
Axis Parameter | Data Type | Units | Meaning |
Hookup Test Status | USINT | - | Returns the status of the last Run Hookup Test service on the targeted drive
axis. The Hookup Test Status attribute can be used to determine when the hookup
test service has successfully completed. Conditions may occur, however, that make it impossible for the drive to properly perform the operation. When this is the case, the test process is automatically terminated and a test error is reported that is stored in the Hookup Test Status output parameter. 0 = test process successful 1 = test in progress 2 = test process aborted 3 = test process timed-out 4 = test process faulted 5 = test failed - no feedback 1 counts 6 = test failed - no feedback 2 counts 7-127 = reserved 128 = test not allowed in Axis Test Mode 129-255 = reserved 2 |
Hookup Test Feedback Direction 1 | USINT | - | Reports the direction of axis travel during the last hookup test, as detected by the drive's feedback 1 device. 0 = The drive’s feedback 1 device detected a positive direction, that is, increasing counts. 1 = The drive’s feedback 1 device detected a negative direction, that is, decreasing counts. 2-255 = reserved The value for Hookup Test Feedback 1 Direction, as determined by the hookup test, does not depend on the current feedback, motor, or motion polarity attribute configuration. This value, combined with the user’s definition of forward direction, can be used to configure the various polarity attributes for the correct directional sense. |
Hookup Test Feedback Direction 2 | USINT | - | Reports the direction of axis travel during the last hookup test, as detected by the drive's feedback 2 device. 0 = The drive’s feedback 2 device detected a positive direction, that is, increasing counts. 1 = The drive’s feedback 2 device detected a negative direction, that is, decreasing counts. 2-255 = reserved The value for Hookup Test Feedback 2 Direction, as determined by the hookup test, does not depend on the current feedback, motor, or motion polarity attribute configuration. This value, combined with the user’s definition of forward direction, can be used to configure the various polarity attributes for the correct directional sense. |
If due to improper hookup, or some other problem with the system, the axis feedback fails to detect that axis reaching the configured Motor Encoder Test Increment after moving the axis at least that distance, then abort the test using the MAS instruction and check the encoder wiring.
Commutation Test
The Commutation test only applies to PM motors. This test applies current to the motor to align the rotor and check for proper phasing of a UVW encoder or Hall sensor, if applicable. Finally, the test measures the commutation offset.
TIP:
For linear stages, make sure there is enough travel. If there is not enough
travel, the test produces a fault.
Axis Parameter | Data Type | Units | Definition |
Hookup Test Status | USINT | - | Returns the status of the last Run Hookup Test service on the targeted drive
axis. The Hookup Test Status attribute can be used to determine when the hookup
test service has successfully completed. Conditions may occur, however, that make it impossible for the drive to properly perform the operation. When this is the case, the test process is automatically terminated and a test error is reported that is stored in the Hookup Test Status output parameter. 0 = test process successful 1 = test in progress 2 = test process aborted 3 = test process timed-out 4 = test process faulted 5 = test failed - no feedback 1 counts 6 = test failed - no feedback 2 counts 7-127 = reserved 128 = test not allowed in Axis Test Mode 129-255 = reserved 2 |
Hookup Test Commutation Polarity | USINT | - | Reports if the UVW phasing of the Encoder or Hall Sensor match the phasing of the
Motor. If the motor and UVW commutation phasing do not match the Commutation
Polarity is Normal. If it is determined that the phasing for the motor and commutation device do not
match, this parameter reports that the Commutation direction is Inverted. This
value can be used to configure the Commutation Polarity attribute. 0 = normal 1 = inverted 2-255 = reserved |
Hookup Test Commutation Offset | Real | Electrical Degrees | The Hookup Test Commutation Offset reports the measured commutations offset of a
PM motor during the Commutation Test. This represents the value that must be
applied to the motor position accumulator in order to align the Electrical Angle
signal with motor stator windings. This value can be used to configure the
Commutation Offset attribute. |
Test Status
This parameter returns the status of the last Run Hookup Test service on the targeted drive axis. Conditions may occur that make it impossible for the control to properly perform the test operation. When this is the case, the test process is automatically aborted and a test fault is reported and stored in the Hookup Test Status output parameter. Possible values for Test Status are shown in the table below:
Error Message | Code | Definition |
Test Success | 0 | Test Process has been successful. |
Test In Process | 1 | Test is in progress. |
Test Aborted | 2 | Test Process was aborted by user. |
Test Time-out | 3 | Test Process has exceeded timed out (2 seconds). |
Test Servo Fault | 4 | Test Process Failed due to Servo Fault. |
No Feedback 1 | 5 | Test Process Failed - no feedback 1 counts. |
No Feedback 2 | 6 | Test Process Failed - no feedback 2counts. |
Test not allowed in Axis Test Mode | 128 | Test Process Failed - Axis Test Mode enabled. |
In this transitional instruction, the relay ladder, toggle the Rung-condition-in from cleared to set each time the instruction should execute.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. A major fault can occur if an uninitialized reference or
a reference of incorrect type is passed to the Axis operand. See Common Attributes for operand-related faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
Prescan | The .EN, .DN, .ER, and .IP bits are cleared to false. |
Rung-condition-in is false | The .EN bit is cleared to false if either the .DN or .ER bit is true. |
Rung-condition-in is true | The .EN bit is set to true and the instruction executes. |
Postscan | N/A |
Structured Text
Condition/State | Action Taken |
Prescan | See Prescan in the Ladder Diagram table. |
Normal execution | See Rung-condition-in is false, followed by rung is true in the Ladder Diagram table. |
Postscan | See Postscan in the Ladder Diagram table. |
Error Codes
See Motion Error Codes .ERR for Motion
Instructions.
Extended Error Codes
Extended Error Codes provide additional instruction specific information for the Error
Codes that are generic to many instructions. Motion Error Codes .ERR for Motion Instructions. The
following Extended Error codes help to pinpoint the problem when the MRHD instruction
receives an error message.
Associated Error Code (decimal) | Extended Error Code (decimal) | Meaning |
SERVO_MESSAGE_FAILURE (12) | Process terminated on request (1) | Test execution followed by an instruction to shutdown/disable drive, or a motion stop instruction or a Processor change requests a cancel of the Test. |
SERVO_MESSAGE_FAILURE (12) | Object Mode conflict (12) | Axis is in shutdown. |
SERVO_MESSAGE_FAILURE (12) | Device in wrong state (16) | Incorrect Tune Process order. (SERCOS) |
TEST_PROCESS_ERROR (15) | Motor Feedback Test Prohibited (1) | Axis Test Mode enabled - Motor and Feedback Test is not supported in this configuration. |
Status Bits
MRHD Changes to Status Bits
Bit Name | State | Meaning |
DriveEnableStatus | TRUE | The axis is in Drive Control state. The Drive Enable output is active while the Tuning Profile is running. |
TestStatus | TRUE | The axis is running a testing process. |
Example 1
When the input conditions are true, the controller runs the encoder diagnostic test on Axis1.
Ladder Diagram

Neutral Text Representation for RLL
MRHD(Axis1, MRHD_1, Motor_Encoder);
Structured Text
MRHD(Axis1, MRHD_1, Motor_Encoder);
Example 2
When the input conditions are true, the controller runs the encoder diagnostic test on Axis1 through a reference to it.
Ladder Diagram

Neutral Text Representation for RLL
MRHD(Ref_Axis1, MRHD_1, Motor_Encoder);
Structured Text
MRHD(Ref_Axis1, MRHD_1, Motor_Encoder);
Provide Feedback