Security > Configure Source Protection command

Select the
Configure Source Protection
command to access the
Source Protection Configuration
dialog box. Use the
Source Protection Configuration
dialog box to:
  • Protect and not protect routines and Add-On instructions using Source Key Protection or License Source Protection.
  • Lock and unlock license-protected components.
  • Manage the source key file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal