Context menus
Use context menus to perform operations on canvas, tables, or other interface elements.
TIP:
The available context menu options depend on the selected item protocol.
Canvas
Command | Description |
---|---|
Go to Zone Table | Focuses on the zone in the Zone list. |
View Properties | Opens zone properties. |
Add Device | Opens a dialog to add a device. |
Add Conduit | Opens a dialog to add a conduit. |
Copy | Copies the zone. |
Paste | Pastes the copied zone. |
Delete | Deletes the zone. |
Command | Description |
---|---|
Device Properties | Opens device properties. |
Port Properties | Opens port properties of the device. |
Add Conduit | Opens a dialog to add a conduit. |
Cut | Cuts the device from the zone and enables you to paste the device into a different zone. |
Copy | Copies the device. |
Paste | Pastes the cut or copied device into the zone. |
Go to Zone Table | Focuses on the device in the Zone table. |
Replace Device | Opens a pop-up window to replace the device. |
Delete | Deletes the device from the model. |
Command | Description |
---|---|
Paste | Pastes the copied zone. |
Zones
You can open the context menu for each zone on the list.
Command | Description |
---|---|
View Properties | Opens the properties of the selected zone. |
Copy | Copies the properties of the selected zone. |
Paste | Creates a zone with the same properties as the last copied zone. The new zone has the same name as the original and adds a number in parentheses. The conduits and devices do not transfer from the original zone. |
Delete | Deletes the selected zone. |
Command | Description |
---|---|
Copy | Copies the properties of the selected zone. |
Paste | Creates a zone with the same properties as the copied zone. The new zone has the same name as the original and adds a number in parentheses. The conduits and devices do not transfer from the original zone. |
Go to Zone | Opens the device table of the selected zone. |
Delete | Deletes the selected zone. |
Command | Description |
---|---|
Device Properties | Displays the properties pane of the device. |
Port Properties | Displays the Port Properties of the selected device. |
Cut | Removes the device from the selected zone. You can Paste this device to a different zone. |
Copy | Copies the properties of the selected device. |
Paste |
|
Replace Device | Opens the Deploy Configuration to Replace Device window.This command is active only if the device was already deployed. |
Delete | Deletes the selected device. |
Conduits
Command | Description |
---|---|
View Properties | Opens the Properties pane of the selected conduit. |
Delete | Deletes the selected conduit. |
Devices
Command | Description |
---|---|
Device Properties | Displays the properties pane of the device |
Port Properties | Displays the port properties of the selected device. |
Cut | Removes the device from the selected zone. You can Paste this device to a different zone. |
Copy | Copies the properties of the selected device. |
Paste |
|
Go to Zone | Opens the device table of the zone that has the selected device is assigned. |
Replace Device | Opens the Deploy Configuration to Replace Device window.This command is active only if the device was already deployed. |
Delete | Deletes the selected device. |
Discovery pane
The commands available in this menu depend on the selected item in the topology.
Command | Description |
---|---|
Add | Adds new devices to the selected zone. |
Add Anchor | Anchors a topology node to the root so that it can be easily accessed without browsing the topology tree. |
Driver Configuration | Opens Configure Driver properties . |
View Property | Opens a list of all properties of the selected device. |
Refresh | Refreshes the network topology. |
Delete | Deletes the item from the topology. |
Provide Feedback