OMRON EtherNet/IP station
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Maximum job size in bytes | MaximumJobSizeInBytes | Maximum size of a transmission of tags from the controller (in bytes). 0 = 504 bytes (maximum value). | |
Port | Port | Number of the port used by the TCP-IP connection. It must match the one configured in the controller. | |
Provide Feedback