Implement the main panel into the main window
Create a dynamic link to the main panel in the dynamic panel.
- InProject view, right-clickMainWindow (type)and select .
- Hover-over the panel loader, select , and enterDynamicPanelLoader.
- InProperties, create a dynamic link betweenPaneland .
Provide Feedback