Install a screen reader extension
You can install a screen reader extension to your Chrome browser from the Chrome Web Store. Screen reader extension allows you to select a text or UI element on the web page using a mouse or keyboard and to read it aloud using the built-in text-to-speech (TTS) service.
Follow the instructions to install a screen reader extension to the Chrome web browser:
- Using the Chrome browser, search for Chrome Web Store.Alternatively, paste the following URL in the search bar and pressEnter.
- In theSearch extensions and themesfield, typeScreen Readeror any specific screen reader extension name and search.
- From the search results, select the screen reader extension you want to install.The selected extension’s detail page is displayed.
- ClickAdd to Chrome.A dialog box displays asking the confirmation to install the selected extension.
- ClickAdd extension.You will be notified once the screen reader extension is successfully added to the Chrome browser.
Mange your screen reader extension
Follow the instructions to enable or disable a screen reader extension:
- At the top right corner of the Chrome window, selectCustomize and control Google Chrome[
] > Extensions>Manage Extensions.The Chrome browser displays theExtensionspage. - Using the toggle button, turn on or turn off the extension that you want to manage.
NOTE:
The provided instructions serve as a general guide for accessing FactoryTalk DataMosaix's accessibility features or functions using the screen reader extensions available for Chrome web browser. While these instructions may be relevant to most of the screen reader extensions, the specific installation and usage procedures may vary depending on the browser, operating system, and screen reader combination.
Provide Feedback