Deactivate Features
Perform the following steps to deactivate features:
- On the Management Console, navigate toManage Access>Features.The Features page displays the available features with a short description and the date they were last updated in the feature management platform.
- Turn the toggle button toInactive.The Confirm Deactivation dialog box is displayed.NOTE:When you deactivate a feature, it becomes unavailable to all users of the selected project.
- ClickDeactivate.Deactivate Feature
You will be notified that the selected feature has been successfully deactivated.
Provide Feedback