Supported Fields for the Events Table
The following table provides the supported fields for the Events table:
Column Name | Column Type | Description | Example |
|---|---|---|---|
id | bigint | A server-generated ID for the object. | 454501654069443 |
createdTime | timestamp | Timestamp when event was created. | 2019-09-07T15:50+00Z |
lastUpdatedTime | timestamp | Timestamp when event was updated. | 2019-09-07T15:50+00Z |
externalId | varchar | The external ID provided by the client. It must be unique for the resource type. | CDF_ExternalID |
dataSetId | bigint | The ID of the dataset this asset belongs to. | 7166729101688251 |
type | varchar | Type of the event. For example: 'failure'. | failure |
subtype | varchar | Sub-type of the event. For example: 'electrical'. | electrical |
description | varchar | Textual description of the event. | CDF project: testing_purpose |
source | varchar | The source of the event. | FTDM |
endtime | timestamp | Timestamp | 2019-09-07T15:50+00Z |
startTime | timestamp | Timestamp | 2019-09-07T15:50+00Z |
Provide Feedback