Create relation in asset and timeseries table
Perform the following steps to create relation in assets and timeseries table:
- Drag and drop theassetstable from the left pane to open campus.Drag and Drop Assets Table

- Drag and drop thetimeseriestable from the left pane and place it next to the assets table.Drag and Drop Timeseries Table

- SelectIdfrom theassetsdrop-down list.By default,=symbol is selected in theOperatordrop-down list.
- SelectAsset Idfrom thetimeseriesdrop-down list.Drop-down Selection

Provide Feedback