Watch Position view parameters
The
Watch Position
view includes these parameters:Parameter | Description |
---|---|
Comparator | Indicates the comparator control to which the configuration applies. |
Control | Specifies the watch position mode as:
|
Value | Specifies the comparator value. Valid comparative values are in the range of 0…4,294,967,295. Use this formula for the comparative value:
For example, for 3,000,000,000 - 4,294,967,296 = -1,294.967,296. |
Provide Feedback