Feedback view parameters
The
Feedback
view includes these parameters:
TIP:
These parameters are not available in Run mode.
Parameter | Description |
---|---|
Code Type | Select Binary or Gray (default) for the code type. |
Word Length | Specify the word length in bits. The word length must be in the range of 2…31 bits. The default word length is 13 bits. |
Baud Rate | Choose a baud rate as one of these values:
|
SSI Word Delay Time | Enter an SSI word delay time in the range of 16…65,535 μs. The default delay time is 64 μs. For example, for 40 µs delay, 40000 - 65536 = 25536 µs delay time. |
SSI Word Filter Control | Choose one of the five successive SSI word filter as:
|
SSI Clock | Select to turn the SSI clock on or off. The default value is On. |
Provide Feedback