Fault/Program Action view parameters
The
Fault/Program Action
view includes these parameters:
TIP:
These parameters are not available in Run mode.
Parameter | Description |
---|---|
Reset Counter | Resets the counter. |
Preset Counter | Sets the value of the counter as specified by the Preset words. |
Reset Counter Value | Resets the value of the accumulated (stored) count. |
Parameter | Description |
---|---|
Reset Counter | Resets the counter. |
Preset Counter | Sets the value of the counter as specified by the Preset words. |
Reset Counter Value | Resets the value of the accumulated (stored) count. |
PWM Hold Last State | Retains the device’s output data in the last state. PWM Hold Last State is only enabled when the Counter Type in the Counter view is set to Pulse Width Modulation (PWM).PWM Hold Last State is disabled when:
|
Value | Value is enabled in these conditions:
If these two conditions are present, enter a value from 0 through 95.00 for the PWM value. |
Output | Displays the output to which this configuration applies. |
Force Output | Turns the outputs on. Outputs are turned on only if the Output Enable checkbox is also selected. If the Force Output checkbox is not selected, outputs might be controlled by a compare match or as directed by the PWM settings. |
Output Enable | Turns the outputs on from either a Force On, Force Output, a compare match, or as directed by the PWM setting. If the Output Enable checkbox is not selected, the device turns the output for the channel to Off. |
Diagnostic Speed | Lets short circuit and open wire diagnostics filter at 50 ms to prevent nuisance trips caused by noisy environments. If the Diagnostic Speed checkbox is not selected, diagnostics respond to a fault condition in less than 8 ms. |
Electronic Fuse Select | Disables outputs upon the detection of a fault condition (short circuit or open wire) and latches the output fault status indicator and Fuse Select. To recover from a faulted state, clear the Electronic Fuse Select checkbox and select the Output Enable checkbox. After clearing the Electronic Fuse Select checkbox, a faulted output continues to operate as instructed until the fault is removed. |
Provide Feedback