Counter view parameters
The
Counter
view includes these parameters:
TIP:
These parameters are not available in Run mode.
Parameter | Description |
---|---|
Type | Choose the desired Counter configuration type. The available values are:
|
Store Count Mode | Choose the desired Store Count Mode. The store count feature lets the device store the current count value of the associated counter. Store count is triggered by the state of the Gate/Reset terminal on the device. The stored count value remains until a new trigger pulse is received at the Gate/Reset terminal. When a new trigger pulse is received, the old count value is overwritten by the new value. The available values are:
Store Count Mode is disabled when Counter Type is set to one of these values:
The default value for Store Count Mode is Store Count Disabled when Counter Type is set to one of these values:
The value for Store Count Mode is Null & Disabled when Counter Type is set to one of these values:
|
Rollover | Each of the two counters has one rollover value associated with it. When the rollover value is reached by the encoder/counter, it resets to 0 and begins counting again. The rollover values range from 1...16,777,216 binary. These words set the number of counts the counter will accumulate before rolling over. For example, a value of 1000 will produce a count sequence of: 998, 999, 0, 1, 2... while incrementing or 2, 1, 0, 999, 998... while decrementing. The values are ignored when the device is operating in Rate Measurement mode. Rollover is enabled when Counter Type is set to one of these values:
The default value is 16,777,215 for these counter types. The Output On/Off value in the Windows view must be set and the preset value must be less than or equal to the rollover value.Rollover is disabled when Counter Type is set to one of these values:
|
Preset | Each of the 2 counters has one preset value associated with it. In the encoder or counter modes, the preset value represents a reference (starting) point (or count) from which the device begins counting. It is set to 0 in other modes. The device counts either up or down from the preset value. Preset values range from 0...16,777,215 binary. Preset is enabled when Counter Type is set to one of these values:
The default value is 0 for these counter types. The preset value must be less than the rollover value. Preset is disabled when Counter Type is set to one of these values:
|
Counter Attenuator | Use the counter attenuator to modify the preset value. Counter attenuator values range from 0...255. Counter Attenuator is enabled when Counter Type is set to one of these values:
The default value is 1 for these counter types. Counter Attenuator is disabled when Counter Type is set to one of these values:
The default value is 0 for these counter types. |
Frequency Precision | The Frequency Precision value multiplies the frequency by the value entered in this field. Valid values include:
Frequency Precision is enabled when Counter Type is set to one of these values:
The default value is 1 for these counter types. When the Scaler value is 16, 32, 64, and 128, the Frequency Precision value must be less than or equal to 1. Frequency Precision is disabled when Counter Type is set to one of these values:
|
Filter | Choose a filter frequency for a counter input (Filter A, Filter B, or Filter Z (Gate/Reset)). The filter frequency is only applied to the inputs for the Input Counter that has filtering chosen (a value other than No Filter is selected). By default, all the filters are chosen. Valid selections are:
|
Invert Input Z | Select to invert the Z input value. The default is unchecked. Invert Input Z is enabled when Counter Type is set to one of these values:
Invert Input Z is disabled when Counter Type is set to one of these values:
|
Scaler | Scaling lets the input pulses at the Gate/Reset (Z input) to be divided by a value. Valid values are: 1 (default), 2, 4, 8, 16, 32, 64, 128. When the Scaler value is 16, 32, 64, or 128, the Frequency Precision value must be less than or equal to 1. Scaler is enabled when Counter Type is set to one of these values:
|
Gate Multiplier | There are four choices for how incoming count at the Gate/Reset terminal are scaled. The counter gate interval is set using the time base setting as its time unit and is calculated in this manner:
There is one Gate/Reset input for each of the 2 counters. The Gate Multiplier, when active, functions in one of the available four counter storage modes. You have the option to scale the incoming count at the Gate/Reset terminal. For scaling, the incoming pulses at Gate/Reset are divided by a number in the range of 1, 2, 4, 8, 16, 32, 64 and 128. The product of the Gate Multiplier value and the Time Base value must not exceed 3 seconds (3000 milliseconds). Gate Multiplier is enabled when Counter Type is set to one of these values:
The default value is 1 for these counter types. Gate Multiplier must be set to 0 when the Type is not PWM or Rate Measurement.Gate Multiplier is disabled when the Counter Type value is set to one of these values:
|
Time Base | Sets the fundamental time base for both counters. The resolution is in multiples of 10 ms, with a minimum of 10 ms intervals (10 ms = 10; 1 s = 1000). Time base must be entered when the Pulse Width Modulation (PWM) and rate measurement are configured. The maximum programmed value is 3000 ms (3 s).Time Base is enabled when Counter Type is set to one of these values:
The default value is 1000 for these counter types. Time Base is disabled when Counter Type is set to one of these values:
|
Actual Gate Interval | Actual Gate Interval is a read-only field that displays the product of the Gate Multiplier and the Time Base when the Type is set to Pulse Width Modulation (PWM) or Rate Measurement. The product of the Gate Multiplier and the Time Base must fall within the valid range of 10...3000 ms. |
Provide Feedback