Ptxx Diagnostics view parameters (5034-OA4)

The
Ptxx Diagnostics
view includes these parameters:
Parameter
Description
Fault Exists
Displays whether a fault is present.
Data Uncertain
Displays the module is operating outside the designed operating range, or data is under manual or override control.
AC/DC Mode
Displays the point output mode.
Field Power
(1)
Displays whether field power is present on the point.
Field Power On Timestamp
(1)
Displays the timestamp of the last time field power turned on in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
You can see a valid time or None if no event time was recorded.
Field Power Off Timestamp
(1)
Displays the timestamp of the last time field power turned off in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
You can see a valid time or None if no event time was recorded.
(1) The parameters Field Power, Field Power On Timestamp, and Field Power Off Timestamp are not displayed when the module is in DC mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal