Counters view parameters (5034-IB16, 5034-IB8)
The
Counters
view includes these parameters:
Parameter | Description |
|---|---|
Counter | Displays the counter number to which this configuration
applies. |
Input Filter Time Off → On | Defines how long an Off to On input transition must remain in
the On state before the device considers the transition
valid. |
Input Filter Time On → Off | Defines how long an On to Off input transition must remain in
the Off state before the device considers the transition
valid. |
Preset | Displays the value, set in the output tag Preset, to use for
counter preset. The value can range from
0…2,147,483,647. |
Rollover at Preset | Determines the action that is taken when the input tag Count
reaches the Preset value.
|
Diagnostics | Opens the Diagnostics dialog, which contains diagnostic
information. |
Provide Feedback