Refreshing the Version Control Status of Elements

Version control status information for elements is available from many sources.
  • From the
    Application View
    , refresh the displayed control status for all elements.
  • From the
    Communication View
    and
    Equipment View
    , refresh the displayed control status for projects and controllers.
  • From the
    Application View
    ,
    Communication View
    , and
    Equipment View
    , obtain version control status details by mousing over the version control icons.
  • In the
    Output
    window, display complete status details for an element including its version control status, locked by, locked on, path, user, version time, latest revision, and local revision.
    Task
    Procedure
    Refresh the control status of elements
    From the required view, right-click any element in the structure, point to
    Version Control
    , and then click
    Refresh Status
    .
    Display complete status information for an element
    From the required view, right-click any element in the structure, point to
    Version Control
    , and then click
    Refresh Status
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal