Pausing Projects and Controllers
Pause projects or individual controllers during simulation. Pausing a project affects all controllers running in simulation. Projects or controllers running online cannot be paused. After pausing a project, resume, for example, continue simulation. After pausing a controller, continue. For example, resume simulation or execute one cycle.
Task | Procedure |
|---|---|
Projects | |
Pause a project | From the Simulation menu, click Pause . |
Resume a paused project | From the Simulation menu, click Continue . |
Controllers | |
Pause a controller | From the Simulation menu, click Pause Controller . |
Resume a paused controller | From the Simulation menu, click Continue Controller . |
Execute one cycle for a paused controller | From the Simulation menu, click Execute One Cycle on Controller . |
Provide Feedback