Child SFC POUs
Any Sequential Function Chart (SFC) program organization unit (POU)
may control other SFC POUs. These level units are called child SFC POUs. A child SFC POU is
a parallel unit that can be started, terminated, frozen, or restarted by its parent. The
parent POU and child POU must both be described with the SFC language. A child SFC POU can
have local variables.
TIP:
When using version control,
do not use child SFC POUs. Use only SFC programs and function blocks in the
application.
When a parent POU starts a child SFC, the parent places an SFC token
(activates) into each initial step of the child. This command is described with the GSTART
statement or with the name of the child with the S qualifier. When a parent POU terminates a
child SFC, it clears all the tokens existing in the steps of the child. Such a command is
described with the GKILL statement or with the name of the child and the R qualifier. When a
parent POU starts a child, the parent continues its execution.
When a parent POU
freezes a child SFC, the parent clears all the tokens existing in the child, and keeps their
position in memory. Such a command is described with the GFREEZE statement. When a parent
POU restarts a frozen child SFC, it restores all the tokens cleared when the child was
frozen. Such a command is described with the GRST statement.
Child SFC function block
instances, as for their SFC function block parents, have a maximum number of tokens, unlike
SFC programs whose dynamic behavior limits are set at the controller level. Specify the
tokens limit for an SFC function block in its settings properties.
When using an SFC
function block with an SFC child, access, for read-only purposes, the local values of the
child from its parent by entering the child’s name and the parameter in an action or
transition’s code. Example: to access the
Local1
parameter of an SFC child named
FB_Child
, in an action or transition defined for the SFC function block parent,
write this syntax:FB_Child.Local1
Task | Procedure |
|---|---|
Add a child SFC POU |
|
Move a child SFC POU |
|
Provide Feedback