SoeServiceStatus
The
SoeServiceStatus C
function block provides the status of the Soe service.
IMPORTANT:
Only use the
SoeServiceStatus
function
block in a single processor configuration. Using this function block in a dual or triple
processor configuration stops the application.
TIP:
To enable controller updates, perform a download
operation after adding an
SoeServiceStatus
function block.This function block has these arguments.
Arguments | ||
|---|---|---|
RST | BOOL | TRUE resets all status values to zero |
SSTS | INT | The status of the SOE server |
ERR | STRING(64) | The description of the possible error codes:
|
EVCT | UDINT | The number of events |
EVMX | UDINT | The maximum number of events in the log |
RESN | UINT | The number of the controller |
COND | USINT | The event condition |
VA | UDINT | SOE variable VA |
RFVA | UDINT | Reference variable VA |
RFVL | STRING(32) | Reference variable value |
TMHI | UDINT | Event timestamp (High 32 bits) |
TMLO | UDINT | Event timestamp (Low 32 bits) |
The timestamp is the number of milliseconds since January 1, 1900.
Provide Feedback