Modifying Cycle Timing
While running an application online, for example, connected, the cycle timing for individual controllers can be modified. When modifying cycle timing, view the following cycle timing information from system variables for individual controllers:
Cycle Information | System Variable | Description |
|---|---|---|
True Cycle Time | __SYSVA_TCYTRUECURRENT | The real duration of a cycle |
Current Cycle Time | __SYSVA_TCYCURRENT | The time spent with the virtual machine |
Maximum Cycle Time | __SYSVA_TCYMAXIMUM | The longest period of time used for a current cycle (__SYSVA_TCYCURRENT), since connecting to the controller |
Cycle Overflow | __SYSVA_TCYOVERFLOW | The number of current cycles (__SYSVA_TCYCURRENT) having exceeded the programmed cycle time |
Programmed Cycle Time | __SYSVA_TCYCYCTIME | The defined cycle time for the controller |
The minimum cycle time for an AADvance application is 64 milliseconds. The cycle time for most applications is between 64 and 260 milliseconds, depending on the system size. The cycle time increases during an update or when a new processor is synchronizing.
TIP:
Setting the Programmed Cycle Time to 0 allows the
controller to execute cycles as fast as possible, for example, at a rate close to the True
Cycle Time.
To modify cycle timing
- From theOnlinemenu, clickCycle Timing.TheCycle Timingdialog box displays cycle time information for all controllers defined in the project.
- Select the controller for which to modify the cycle timing, indicate a new programmed cycle time, and then clickUpdate.
- (optional) To refresh the maximum cycle time and cycle overflow information display for controllers, clickReset all Statistics.
Provide Feedback