Multiplication
Multiplies 2 to 127 integer or real variables.

Arguments | ||
|---|---|---|
(inputs) | SINT - USINT - BYTE - INT - UINT - WORD - DINT - UDINT - DWORD - LINT - ULINT - LWORD - REAL - LREAL | All inputs must have the same format. From 2 to 127 inputs. |
output | SINT - USINT - BYTE - INT - UINT - WORD - DINT - UDINT - DWORD - LINT - ULINT - LWORD - REAL - LREAL | Multiplication of the input variables. |
Example
(* FBD example with Multiplication Operators *)

(* ST equivalence *)
ao10 := ai101 * ai102; ao5 := (ai51 * ai52) * ai53;
Provide Feedback