ANY_TO_SINT
Converts variables 8-bit short integer variables

Arguments | ||
|---|---|---|
i1 | BOOL - SINT - USINT - BYTE - INT - UINT - WORD - DINT - UDINT - DWORD - LINT - ULINT - LWORD - REAL - LREAL - TIME - DATE - STRING | Any value |
o1 | SINT | 0 if i1 is FALSE / 1 if i1 is TRUE number of milliseconds for a timer integer part for real decimal number represented by a string |
Example
(* FBD example with "Convert to Short Integer" Operators *)

(* ST Equivalence: *)
bres := ANY_TO_SINT (true); | (* bres is 1 *) |
tres := ANY_TO_SINT (t#0s46ms); | (* tres is 46 *) |
mres := ANY_TO_SINT ('0198'); | (* mres is 198 *) |
Provide Feedback