ANY_TO_REAL
Converts variables to REAL variables

Arguments | ||
|---|---|---|
i1 | BOOL - SINT - USINT - BYTE - INT - UINT - WORD - DINT - UDINT - DWORD - LINT - ULINT - LWORD - REAL - LREAL - TIME - DATE - STRING | Any value |
o1 | REAL | 0.0 if i1 is FALSE / 1.0 if i1 is TRUE number of milliseconds for a timer equivalent number for integer |
Example
(* FBD example with "Convert to Real" Operators *)

(* ST Equivalence: *)
bres := ANY_TO_REAL (true); | (* bres is 1.0 *) |
tres := ANY_TO_REAL (t#1s46ms); | (* tres is 1046.0 *) |
ares := ANY_TO_REAL ('198'); | (* ares is 198.0 *) |
Provide Feedback