ANY_TO_DATE
Converts variables to DATE variables. A 32-bit variable, providing the number of seconds since Jan 1, 1970, based on the time_t data type.

Arguments | ||
|---|---|---|
i1 | BOOL - SINT - USINT - BYTE - INT - UINT - WORD - DINT - UDINT - DWORD - LINT - ULINT - LWORD - REAL - LREAL - TIME - DATE - STRING | Any value |
o1 | DATE | date represented by i1. A value of -1 indicates an invalid date. |
Example
(* FBD example with "Convert to DATE" Operators *)

(* ST Equivalence: *)
ares := ANY_TO_DATE (1109110199); | (* ares := d#2005-02-22 *) |
rres := ANY_TO_DATE (1109110199.3); | (*rres := d#2005-02-22 *) |
Provide Feedback